How to use LabVIEW for FPGA Based Application

Figure 1: General block diagram to program FPGA

How to use LabVIEW for FPGA based application

You can use LabVIEW to program a FPGA through the LabVIEW FPGA add-on module and design FPGA-based systems more effectively and efficiently through a highly integrated development environment that has IP libraries, a high-fidelity simulator, and debugging features. It helps develop FPGA VIs that combine direct access to I/O with user-defined LabVIEW logic to define custom hardware for applications such as digital protocol communication, hardware-in-the-loop simulation, and rapid control prototyping. It contains many integrated signal processing routines. You can also incorporate existing hardware description language (HDL) code as well as third-party IP. Use this module to program various NI-specific hardware like CompactRIO Systems (cRIO), FlexRIO, PXI Multifunction Reconfigurable I/O Module, Industrial Controllers, etc. Figure 1 shows a general block diagram to program NI FPGA hardware using LabVIEW.

Figure 2: Hardware connection

Figure 1: General block diagram to program FPGA

To illustrate, we will connect a cRIO-9076, an industrial embedded controller from NI, to control and monitor applications. It features a real-time processor and a Xilinx Spartan-6 LX 45 FPGA with Ethernet, USB, and serial connectivity ports. For input and output, we will use NI-9421, 8- channel digital input module, and NI-9474, 8-channel digital output module, which is used with the cRIO module. Each channel is compatible with 24 V logic levels and has an LED indicating the state of that channel.

The following steps create an FPGA application that accepts a digital input and generates two digital outputs toggling each other in high and low logic levels. The application is implemented on the host LabVIEW machine, compiled, and deployed on the cRIO-9076 FPGA machine.

Hardware Connections:

As shown in figure 2, hardware connections are made where the input and output module has been plugged into the cRIO chassis slot. A 24VDC power supply is connected to the DI0 channel of the input module in series with a toggle switch. The output module is powered through 24VDC, and output can be checked on the DO0 and DO1 channels of the output module. Connect host PC to cRIO chassis with a network cable (blue cable in the figure).

Figure 3: LabVIEW FPGA project window

Figure 2: Hardware connection

To implement the LabVIEW program, we need to install LabVIEW, LabVIEW FPGA Module, LabVIEW Real-Time Module, and NI-RIO Driver on the windows based host PC.

LabVIEW Program:

Execute the following steps to write the LabVIEW program.

Open LabVIEW application and create LabVIEW FPGA project, which will detect connected hardware and open project window as shown below.

Figure 4: Blank FPGA VI window

Figure 3: LabVIEW FPGA project window

This project window includes two categories: My Computer, which is to create an application on host pc, and c-RIO-9078 (169.254…) which is to make an application on target RT machine (cRIO-9076). Now navigate to cRIO-9076->Chassis (cRIO-9076)->FPGA Target (RIDO, cRIO-9076), do right-click, and create a new VI that will open the window as shown below figure. The code on this VI will run directly on the target machine.

Figure 5: Writing LabVIEW code

Figure 4: Blank FPGA VI window

FPGA target has built-in sub-VI to access its input and output channels like Mod1 and Mod2. Navigate to cRIO-9076->Chassis (cRIO-9076)–Mod1 and cRIO-9076->Chassis (cRIO-9076)–Mod2 and drag sub-VI Mod1/DI0, Mod2/DO0 and Mod2/DO0 on the block diagram and connect as shown in figure 5. Enclose the code in a while-loop, and to continuously run it, connect the control to FALSE (F) Boolean Constant. The code shows that when we input DI0 at high logic (24V), the DO0 will be low and DO1 high. With the low input, it will be reversed.

Figure 6: Compiling code on target

Figure 5: Writing LabVIEW code

After completing the code, click on the “RUN” button, which opens a new window for compiling the code on the target machine. Select the “Connect to LabVIEW FPGA Compile Cloud Service” giving NI credential and click Ok.

Figure 7: Status window after compilation

Figure 6: Compiling code on target

After successfully compiling the code, it will open the status window (figure 7). After this message, the target is ready to execute the application having running code.

Figure 7: Status window after compilation

Now, giving the input signal through the toggle switch will show status as below the truth table.

DI0DO0DO1
HighHighLow
LowLowHigh

High level = 24V

Low level = 0V

Applications

Internet of Things

Internet des objets

Artificial Intelligence

Intelligence artificielle

Industrial Automation & Control

Automatisation et contrôle industriels

Transportation

Transport

Healthcare

Healthcare

Robotics

Robotics

Maintenance & Safety

Maintenance et sécurité

Alternative Energy

Alternative Energy

Autres ressources

Calculatrices et tableaux de conver
Guides de sélection et catalogues
Modules d’apprentissage essentiels
Pleins feux sur la technologie
Ressources de conception
Glossaire d’ingénierie
Technical Support
Parts Finder Tools