Securing connected devices: challenges & solutions

In today's technologically advanced world, connected devices have become integral to our daily lives. Connected devices, also known as Internet of Things (IoT) devices, offer seamless connectivity and automation in anything from smartphones and smart TVs to smart household appliances and industrial machinery

Introduction

In today's technologically advanced world, connected devices have become integral to our daily lives. Connected devices, also known as Internet of Things (IoT) devices, offer seamless connectivity and automation in anything from smartphones and smart TVs to smart household appliances and industrial machinery. These devices have sensors, processors, and network connectivity, allowing them to collect and transmit data to perform various functions. The increasing number of linked devices has resulted in various advantages, including enhanced effectiveness, convenience, and productivity. However, ensuring their security has become essential with an increasing number of technologically advanced devices. Securing connected devices is essential for safeguarding user privacy, protecting key infrastructure, and maintaining consumer and business competence. This article will look at the security challenges connected devices encounter in wireless and wired connectivity networks and effective solutions for mitigating these threats.

Importance of security in connected devices

  • Data security and privacy: Connected devices collect and transmit sensitive personal and organisational data, such as personally identifiable information (PII), financial data, and proprietary business information. Without strong security safeguards in place, this data is vulnerable to unauthorised access, theft, and abuse, resulting in privacy violations and financial losses.
  • Physical security and safety: Connected devices are being incorporated into key infrastructures such as healthcare systems, transportation networks, and industrial control systems. Any security breach in these devices can potentially threaten human lives, interrupt services, or cause substantial physical damage.
  • Reputation and trust: Security breaches involving connected devices can have serious ramifications for manufacturers, service providers, and customers. Data breaches, malware infections, and unauthorised access may erode consumer trust and harm a brand's reputation, resulting in financial losses and lower customer engagement. To know more about open platform communication click here.

Security challenges in connected devices

Despite increasing awareness of safety risks, various obstacles remain in connected devices. Understanding these issues is critical for building viable solutions. Here are some examples of common security challenges:

  1. Lack of standardisation: One of the major safety concerns in IoT is a lack of standardisation. Ensuring compatibility and interoperability is difficult With so many devices, protocols, and platforms. This can result in vulnerabilities that attackers can exploit.
  2. Insufficient authentication and authorisation: Another key issue confronting IoT is the prevalence of weak or insufficient authentication techniques in connected devices. Many devices continue to utilise default credentials or weak passwords, exposing them to unauthorised access. Inadequate authorisation methods exacerbate the situation by enabling unauthorised users access to critical functions.
  3. Vulnerabilities in software and firmware: IoT devices are frequently powered by embedded systems with limited resources, making them challenging to protect. This can result in vulnerabilities that attackers can exploit. Furthermore, embedded systems frequently include specialised hardware and software, which might provide extra issues when it comes to security.
  4. Physical security risks: IoT devices have significant physical security challenges since they are frequently small and simple to conceal, leaving them vulnerable to physical assaults. Tampering, theft, or destruction of an IoT device are examples of physical attacks. This can lead to unauthorised access to sensitive data, system outages, and data loss.

Solutions for security challenges

A multi-layered approach is necessary to handle security challenges in connected devices successfully. Here are some solutions that can significantly enhance the security of connected devices:

Standardisation and regulation

  • Developing and implementing industry standards for IoT devices, protocols, and platforms can aid in ensuring compatibility and interoperability. This might include device security standards, data privacy standards, and communication protocols.
  • IoT device and platform certification can assist verify that they accomplish certain safety criteria. This may help organisations gain trust in the security of the devices they use, as well as identify devices that may be more vulnerable to attack.
  • Using a secure gateway may assist ensure that all network devices communicate securely. A secure gateway, for example, may be used to encrypt communications, authenticate devices, and monitor network traffic for unusual activities. This can help reduce the risk of attacks and improve network security overall.

Strong authentication and authorisation mechanisms

  • Implementing strong methods of authentication, such as two-factor authentication, to ensure that only authorised users have access to the device can support.
  • Using a secure gateway will ensure that all network devices communicate securely.
  • Using Public Key Infrastructure (PKI) can help ensure the authenticity of all network devices. And secure data transfer technologies such as Transport Layer Security (TLS).

Regular software and firmware updates

  • Using safe IoT app development practises such as threat modelling and code reviews may assist assure software security. Organisations may assist to lower the risk of attacks and improve the security of their IoT devices by adding these practises into the development process.
  • Using secure boot and secure firmware update protocols can assist to ensure that reliable software is running on the device. Secure firmware update techniques may verify that the device is running the most recent firmware version, as well as that any upgrades are genuine and have not been tampered with.

Implementation of physical security measures

  • Using secure network protocols such as VPN and HTTPS will help ensure secure information transmission. Virtual Private Networks (VPNs) may be used to encrypt connections between IoT devices and the internet, making data interception more difficult. HTTPS, on the other hand, may be used to encrypt communications between web servers and clients, adding a further level of protection to web enabled IoT devices.
  • Using network segmentation may help reduce the impact of a network assault. To limit the scope of an attack, network segmentation involves separating a network into smaller sub-networks, or segments. An organisation, for example, may segment its network such that all IoT devices are on a distinct segment from the rest of the network.
  • Since the attacker can only access the segment retaining the IoT devices rather than the entire network, this will help in limiting the impact of an attack on IoT devices

To know more about IoT in industrial-connected devices click here.

Best practices for connected device security

  1. Password management: Encouraging users to use strong and unique passwords, as well as changing passwords on a regular basis, is essential. Utilising password managers and enabling two-factor authentication improves device security significantly.
  2. Network security: It is critical to maintain strong network security. This includes employing strong encryption methods such as WPA2/WPA3, segmenting networks, implementing firewalls, and monitoring network traffic on a regular basis to detect any irregularities or unauthorised access attempts.
  3. Encryption: Implementing end-to-end encryption for data transport and storage ensures that sensitive information remains secure even if intercepted. Both data in transit and data at rest on linked devices should be encrypted.
  4. Regular auditing and monitoring: Regular auditing and monitoring operations enable organisations to proactively detect and respond to possible security issues. Analysing device logs, monitoring network traffic, and employing intrusion detection systems all contribute to the continued security of linked devices.

Conclusion

As the number of connected devices diversifies, it becomes increasingly important to prioritise their security. The risks involved with compromised devices can have serious ramifications for people, businesses, and society. We may mitigate these risks and fully utilise the promise of connected devices by recognising security concerns and developing effective solutions. Manufacturers, developers, and end users must work together to create a secure and resilient ecosystem for connected devices, assuring a safer and more trustworthy digital future.

Farnell has partnered with many different suppliers catering to a wide range of edge device mesh networking components portfolio, such as internet of things, IoT solutions Kits, wireless modules & adaptors, communications & networking modules, bluetooth modules & adaptors, zigbee modules / XBee, WLAN modules & USB adaptors, industrial wireless, RF / wireless development kits, and networking - wireless products.