What is Han-Modular®?
With the Han-Modular® series, you can optimally design connectors to supply machinery and equipment. This is made possible by combining individual modules for different transmission media. The connector handles different signal types through the combination of different modules that the designer selects. Modules can also be used to accommodate multimedia types, such as power, signal, and data can be combined into a single connector rather than separate connections.
Explore the Benefits of Modular Connectors
- Space Savings
- Integration of multiple connectors into a single unit allow for significant reduction in space requirements.
- Low-Maintenance
- Using a pre-assembled, pre-tested connector assembly can reduce hard wiring and installation time.
- Flexibility
- With the Han-Modular® series, users can assemble their ‘own’ connectors according to their own individual requirements. Essentially creating a “custom” connector using standard stocked modules.
- Future Proof
- Placeholder modules give you the flexibility to future-proof your modular connector design.

Check Out Our Featured Content
Hardwire vs. Connectors
When deciding between the two options, there are several considerations to think about.
Find out how to choose by reading the White Paper!
Frequently Asked Questions
What is a modular connector?
What kind of machine automation applications would replace hardwired connections with a modular connector?
How does the configuration process for a modular connector begin?
Is there a maximum or minimum physical size for modular connectors?
Is there a maximum number of conductors that modular connectors can handle?
What kind of connections can modular connectors handle?
What are the limits on the connection parameters?
What kind of quality standards apply to modular connectors?
What determines whether a connector needs a lock?
Can connectors be water tight?
Can connector housings be plastic or metal?
Are there special factors that bear on connectors that combine different signal types?
Circular vs. Rectangular

You twist circular connectors into place & lock rectangular connectors with latching mechanisms.
Discover which one you should use!
Frequently Asked Questions
What kinds of connectors can engineers specify for machine designs today?
Why are circular connectors so common, if they pose drawbacks?
How are today’s connectors different than those in the past?
What are the main benefits of rectangular connectors?
Key advantages for using rectangular connectors over circular include:
- Off-the-shelf modules for easy, custom designs for any application
- Superior space efficiency
- More termination options – crimp, solder, screw terminal, others
- More locking options - single or double -lever and push button
- Ability to connect to other devices such as a PCB
- Greater contact density possible
- Greater cabling flexibility – top, dual, side or angled cable entry
- Surface mount, panel mount and cable -to -cable compatibility
- Lower cost
- Better protection against overvoltage
- Easier visual mating
Which connectors are more reliable?
What other challenges does the connector market face?
Do rectangular connectors provide other electrical benefits?
In contrast, a PE connection in circular connectors is not a standard feature. It can be added, but it will be a costly option. Since there is a limited number of pin configurations, only a specific pin can function as ground, and there is only one contact gender per side.
What does the future hold for rectangular connectors?